Can I use a NTP Server to synchronize the clock of my controller?

  1. Home
  2. Knowledge Base
  3. FAQs
  4. Can I use a NTP Server to synchronize the clock of my controller?

Summary

Is it possible to sync the RC8/RC8A controller clock using an NTP server?

Answer

There is no feature to sync the clock of the RC8 controller via an NTP but you are able to read the current time using the following commands:

– Now Command: https://www.fa-manuals.denso-wave.com/en/usermanuals/000390/
– Time Command: https://www.fa-manuals.denso-wave.com/en/usermanuals/000387/


Was this article helpful?

Related Articles