HS Series Preventive Maintenance and Inspection

  1. Home
  2. Knowledge Base
  3. Robot Arms
  4. HS Series Preventive Maintenance and Inspection

Interval and Purposes

Carry out the maintenance and inspection jobs listed in the table below.

Caution

Maintenance and inspection must be carried out by a trained worker who possesses the ability to perform these tasks safely.

Before performing maintenance and inspection jobs, read the SAFETY PRECAUTIONS, “Precautions while Robot is Running 1 ” and “Others “.


No.

Interval

Purpose
1DailyTo use your robot safely.
2QuarterlyTo maintain the precision of the robot and to prevent failures caused by overheat of the robot controller
3Semiyearly To check the rotary sections and slideways of the robot and its controller for wear, preventing seizure, breakage, and other serious failures that could result from wear.
3BiennialTo retain the position data stored in the electronic absolute encoder built in the robot unit.
Replace backup batteries as specified in every two years.

Owner’s Manual Reference

https://www.fa-manuals.denso-wave.com/en/usermanuals/006066/


Was this article helpful?

Related Articles