I need EDS file for DeviceNet

  1. Home
  2. Knowledge Base
  3. Fieldbus Communication
  4. I need EDS file for DeviceNet

An EDS file, which is read in the network configuration software, is used to establish, manage, and design networks on your PC. There are several ways to obtain a copy of this file:

DENSO Wave site

You can find a copy of the EDS file for the RC8 controller and other models on our DENSO Wave site.

https://www.denso-wave.com/en/robot/download/application/j1eds.html

Directly from the robot controller (Applies to RC8 / RC8A / COBOTTA)

  1. Make sure that you know your controller’s IP Address and that your PC has and IP Addres that is within the same network as your controller.
  2. Open a Web browser and go to the following addess http://<RC8 IP Address>/eds/. Replace <RC8 IP Address> for the IP address of your controller for example 192.168.0.1
  3. Download the file denso_RC8_eia_V1.1.eds
This image has an empty alt attribute; its file name is image.png

You can also obtain a copy of the EDS file from by connecting to the controller

Please consult the owner’s manual for more details and latest information on EDS file and DeviceNet https://www.fa-manuals.denso-wave.com/en/usermanuals/005836/

Was this article helpful?

Related Articles