VS Series Encoder Battery Replacement

  1. Home
  2. Knowledge Base
  3. Robot Arms
  4. VS Series Encoder Battery Replacement

Overview

The encoder built in the servomotor stores position data. To prevent the position data from being lost, the encoder backup batteries supply power to the encoder memory.
Periodically replace the encoder backup batteries that are loaded in the robot unit. In the event of using the external battery unit, replace the battery of the external battery unit.

This procedure applies to the following robot types: VS-050, VS-060, VS-068, VS-087

Tools and Parts needed

  • Philips-Head screwdriver
  • Encoder backup battery for VS series robots.
    • 410679-0010 – Encoder backup battery

Note:
If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.

Video Tutorial

Step by Step Guide

Step 1

Make two new backup batteries ready for use.

Step 2

Turn the controller power OFF.

Step 3

Remove the cover from the Encoder Backup Battery Box.

Note:
Protected type robots (IP67) or Dust- & splash-proof type robots (IP54) have an O-ring on the inside of the cover. Take care not to break the O-ring.

VS-050 / VS-060
VS-068 / VS087
External Battery Unit option

Step 4

Replace the backup batteries using the procedure below.

First join the connector of a new battery to an empty connector on the robot unit, disconnect and remove the old battery, then load the new one.

NOTE:
During replacement, at least one battery should be connected. Disconnecting all batteries loses position data.
Be sure to replace all batteries with new ones at one time. Using old and new batteries together shortens the service life.

Step 5

Put the cover back to the Encoder Backup Battery Box.

Tightening Torque

Standard type robots (IP40) 0.6 +/- 0.1 Nm
Other than standard type (IP40) 1.6 +/- 0.2Nm
External Battery Unit1.6 +/- 0.3 Nm

Next Steps:

Owner’s Manual Reference

https://www.fa-manuals.denso-wave.com/en/usermanuals/000069/


Was this article helpful?

Related Articles