Robots revolutionized the industry over twenty years ago. However, today’s industrial robots are so much better than the ones first used to replace human laborers. In fact, one articulated robot is able to do more work with greater skill than a similar bot two decades old. Here’s why today’s articulated robot is better.
Greater Range of Motion and More Precision
With the increased articulation and rotation, these industrial robots have a greater range of motion and are much more precise in their tasks. It means that the robotic arms can move in all directions, something a human arm can’t. Similar robotic arms could not perform the same range of motion years ago, and the movements of the older bots were often jerky at best. Now the new robots move with fluid movement and can place components on a computer board the size of pin heads.
Less Need for Human Attendants
Older robots needed human attendants in case they got stuck or jammed up. The modern and more recent versions don’t need much if any, human help at all. That’s good news if you want to automate as much of your factory as possible. One or two repair technicians can remain in your employment while the robots do all the rest of the work more efficiently and with greater speed.
If you would like a demonstration of these modern industrial robots in action, or you just want to know more about how automation in your plant works, contact DENSO Robotics via https://www.densorobotics.com today.